Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

Now at Mouser: Texas Instruments Sitara AM574x Processors for High-Performance Embedded Applications

October 17, 2019 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the Sitara™ AM574x processors from Texas Instruments (TI). These Arm® Cortex®-based devices achieve high levels of processing and are designed to meet the intense processing needs of modern embedded applications, including industrial communications, human-machine interface (HMI), and automation and control.

TI Sitara AM574x processors, available from Mouser Electronics, incorporate dual-core Arm Cortex-A15 reduced instruction set computer (RISC) CPUs with Arm Neon™ extensions and two TI C66x floating-point DSP cores. The processors include dual Programmable Real-time Unit for Industrial Communications sub-systems (PRU-ICSS) that can be used for industrial Ethernet protocols such as Profinet, EtherCAT, and Ethernet/IP. The devices also combine programmable video processing with a highly integrated peripheral set, offer up to two embedded vision engines (EVEs), and include cryptographic acceleration.

The devices integrate a robust Image and Video Accelerator - High Definition (IVA-HD) subsystem with support for 4K at 15 fps, encode and decode support for H.264 CODEC, a 2D graphics accelerator, and a dual-core 3D GPU. Other features include two-port Gigabit Ethernet, a general purpose memory controller, enhanced direct memory access (EDMA) controller, sixteen 32-bit general-purpose timers, and a 32-bit MPU watchdog timer.

The Sitara AM574x processors are supported by the TMDSIDK574 Industrial Development Kit (IDK), a standalone test, development, and evaluation module that enables developers to write software and develop hardware for industrial control and industrial communications applications. The TMDXIDK574 breaks out six Ethernet ports, four of which can be used concurrently: two Gigabit Ethernet ports and two 10/100 Ethernet ports from the PRU-ICSS subsystems.

The TMDXIDK574 IDK also includes connectors for Mini PCIe, USB 3.0, and HDMI and support for an optional TMDXIDK57X-LCD touchscreen display. The kit offers a defined set of features to allow developers to experience industrial communication solutions using various serial or Ethernet-based interfaces. Using standard interfaces, the TMDXIDK574 IDK may interface to other processors or systems and act as a communication gateway or controller. In addition, it can directly operate as a standard remote I/O system or a sensor connected to an industrial communication network.

To learn more about the Sitara AM574x processors, visit www.mouser.com/ti-am5746-am5748-am5749-processors.


With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 800 manufacturers. Mouser offers 27 support locations around the world to provide best-in-class customer service and ships globally to over 630,000 customers in more than 223 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room