NXP's KW39/38/37 Wireless Microcontrollers, Now at Mouser, Expand Bluetooth Long Range Capabilities
July 7, 2020 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the KW39/38/37 families of wireless microcontrollers from NXP Semiconductors.
NXP KW39, KW38, and KW37 families of wireless microcontrollers are highly integrated single-chip devices that enable Bluetooth® Low Energy and generic FSK connectivity for automotive and industrial embedded systems. The KW39/38/37 are fully AEC Q100 Grade 2 automotive and industrial qualified. The devices integrate an Arm® Cortex®-M0 CPU with up to 512 KBytes of flash and 64 KBytes of SRAM. The microcontrollers feature -30 dBm to +5 dBm programmable transmitter output power, low external component count for low-cost application, and on-chip balun with single-ended bidirectional RF port.
Developers can use the KW39/38/37 devices as a "BlackBox" modem to add Bluetooth Low Energy or Generic FSK connectivity to an existing host microcontroller or microprocessor, or as a standalone smart wireless sensor with embedded application where no controller is required. The integrated DC-DC converter enables operation from a single coin cell lithium-ion battery, enabling a significant reduction of current consumption for power-critical applications. These microcontrollers feature an operating voltage range of 1.71 V to 3.6 V and an operating temperature range of minus 40 degrees to 105 degrees Celsius.
The target automotive applications for the KW39/38/37 devices include include car access and car sharing, passive entry/passive start (PEPS) systems, sensors, and wireless on-board diagnostic functions. Industrial applications include asset tracking, building control and monitoring, CAN-to-Bluetooth Low Energy bridges, and data usage collection.
To learn more, visit https://www.mouser.com/new/nxp-semiconductors/nxp-kw39-38-37-wireless-mcus/.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 800 manufacturers. Mouser offers 27 support locations around the world to provide best-in-class customer service and ships globally to over 630,000 customers in more than 223 countries/territories from its 1 million sq. ft. state-of-the-art facilities south of Dallas, Texas. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com