New at Mouser: NXP Semiconductors NTAG X DNA Secure Connected NFC Tag for IoT, Consumer, and Medical Applications

New Product Announcement

Connect With Us


Learn more about the NTAG X DNA secure connected NFC Tag
Learn more about the NTAG X DNA secure connected NFC Tag

January 26, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new NTAG® X DNA secure connected NFC tag from NXP® Semiconductors. The NTAG X DNA NFC tag is designed to securely verify the authenticity of a product prior to purchase, combat counterfeits, and help manufacturers meet Digital Product Passport (DPP) security, trust, and integration requirements for IoT, consumer, and medical applications.

The NXP NTAG X DNA Type 4 NFC tag, available from Mouser, leverages 16KB of high-density memory, a high data rate, and secure unique NFC (SUN) authentication to quickly and securely verify a product or device's authenticity. The NTAG X DNA enables mobile devices to securely transfer data to another device via I2C or an NFC interface, utilizing ECC key pairs, which the IC  generates, to ensure that private keys are never exposed outside the IC. Additionally, supported by NXP's EdgeLock® 2GO credential delivery service, NTAG X DNA offers a highly secure authentication experience.

The NTAG X DNA NFC Tag conducts cryptographic operations for security-critical communication and control functions utilizing Common Criteria EAL 6+ security certification with AVA_VAN.5 on the product level, and supports a generic Crypto API supplying AES, ECDSA, ECDH, SHA, HMAC, and HKDF cryptographic functionality. Asymmetric cryptography allows support for 256-bit ECC over the NIST P-256 and brainpoolP256r1 curves, while symmetric cryptography supports both AES-128 and AES-256 and facilitates PKI-based mutual authentication, including certificate handling. The NTAG X DNA hosts an I2C contact interface with two GPIOs and an ISO 14443 contactless interface. The device delivers a low-power design and consumes only 5μA in halt mode when an external VDD is equipped.

To learn more about the NTAG X DNA Secure Connected NFC Tag, visit https://www.mouser.com/new/nxp-semiconductors/nxp-ntag-x-dna-nfc-tag/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About NXP Semiconductors

2026 - NXP Semiconductors enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security and privacy and smart connected solutions markets.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764