Audio Analytics: From Sound Capture to Edge AI Events
Image Source:
Olga Gorkun/Stock.adobe.com; generated with AI
By Traci Browne for Mouser Electronics
Published March 9, 2026
Not long ago, audio analytics meant offline processing of recorded clips to search for keywords, measure levels, or tag events after the fact. Today, the industry is moving more toward artificial intelligence (AI)-powered edge analytics to detect key sounds without requiring audio streaming.[1]
For example, a building security system might use audio analytics to detect abnormal sounds, such as breaking glass and shouting, triggering instant alerts. Because the system classifies sounds instead of storing raw audio, it reduces privacy risks while enabling quick intervention.
Edge analytics are spurring a shift that requires system-based thinking, as the work extends far beyond algorithm development. Think of this as an audio analytics pipeline that combines sound, video, Internet of Things (IoT) sensors, and edge computing, enabling cameras and smart microphones to process events in real time and send only the data that matters.
The Audio Analytics Pipeline
Audio analytics appears in many environments, but the underlying pipeline is consistent. The system captures sound, digitally represents it, and analyzes it locally to generate usable events. Consider this audio analytics pipeline in a video call.
Stage 1: Capturing and Conditioning Sound
During the video call, the microphone cannot distinguish a user’s voice from a dog barking in the background. It simply detects a single changing air-pressure pattern.
In this first part of the pipeline, the microphone converts changes in air pressure into an electrical signal, with the voltage rising or falling as the overall sound level increases or decreases.
The audio front end then applies simple filters to remove low-frequency hum and high-frequency interference. Gain is set so that normal speech sits above background noise, but not so high that loud sounds clip and distort the signal.
Once the filters “clean” the signal, the analog-to-digital converter (ADC) transforms it into a stream of digital samples that the system can process (Figure 1).
Figure 1: The process of capturing and conditioning sound. (Source: Author/Mouser Electronics)
Stage 2: Extracting Audio Features
The digital audio samples are clean, but simply inspecting each raw sample value on its own is not enough. Instead, the system chops the signal into small time slices and, for each slice, computes summary features, such as overall amplitude, energy distribution across frequencies, and amount of energy within the frequency range typical of human speech.
Each slice becomes a compact feature vector, and the software uses these vectors to distinguish speech from sounds like a dog bark and to detect when someone starts or finishes speaking. With these higher-level features, the device can run echo cancellation, noise suppression, and voice activity detection in real time (Figure 2).
Figure 2: The process of extracting audio features. (Source: Author/Mouser Electronics)
Stage 3: Turning Features into Events
Once that feature stream exists, labeling begins. The system needs to determine which participants are speaking and when to change the video focus point, while also labeling and blocking background noise to distinguish it from speech. But what if the implementation was more sophisticated, such as in a call center environment?
A call center implementation would produce different requirements. In this situation, supervisors want to know if a caller is getting frustrated. The models rely on features like volume, tone, and speech speed to predict emotional states and speech tension. As the system matures, the output shifts from simple signal views to higher-level events that drive dashboards and workflows (Figure 3).
Figure 3: A visual representation of the turning features into events process. (Source: Author/Mouser Electronics)
Where the Pipeline Runs: Edge vs. Cloud
As previously mentioned, audio analytics systems like this no longer rely only on high-performance processors and cloud-based infrastructure. Complex models for full transcription, advanced sentiment analysis, and long-term trend monitoring still run on PCs and servers, but they now start from a feature and event stream that originates on the device. In many modern headsets, smart speakers, and conferencing soundbars, the microphone sends signals to digital signal processing (DSP)-enabled microcontrollers (MCUs) or dedicated DSP chips. These devices handle front-end cleanup, extract features, and make basic speech-presence decisions before any data leave the hardware.
Why Front-End Choices Make or Break Analytics
For electrical design engineers, these front-end choices determine how well the entire analytics pipeline performs. Every downstream decision depends on what the front end delivers. Microphone selection and placement, analog gain configuration, filtering, and converter settings determine the noise level, operational range, and delay, all of which affect all analytical operations.
When these pieces are implemented well, the same hardware platform can support everything from simple noise reduction in consumer devices to real-time analytics in headsets, smart speakers, and video cameras.
Detecting Health Events Without Recording Speech
For another example scenario, consider a ceiling-mounted system designed to detect coughs in a hospital room. The audio front end must extract cough signals from room sounds that include noise from background equipment and heating, ventilation, and air conditioning (HVAC) systems, and it needs to run continuously. Because of strict patient privacy laws, the system must be built for on-device inference so that it transmits only event metadata, rather than a continuous raw audio stream.
Such a system might incorporate a small array of low-power microelectromechanical (MEMS) microphones to provide adequate coverage. Gain is set so quiet coughs stand out from background noise, and so that loud, unexpected sounds do not drive the signal into clipping. The front end filters out hum and HVAC rumble while preserving frequencies associated with cough sounds. Mechanical designers position the microphones away from screws and vents to prevent vibration and airflow artifacts.
A low-power, always-listening stage monitors the signal for cough-like patterns, which then trigger a more powerful processor to analyze short clips. This capability keeps the device within power and thermal budgets while hospital policies ensure only event data (e.g., time, room number, cough detected) leave the device.
Listening for Stress Signals in Call Center Audio
In a call center scenario, a headset is part of a system that alerts supervisors when individual calls begin to deteriorate, so they can quickly intervene. The audio front end must capture clear speech in a noisy room, run continuously on a low-power device, and support privacy controls so analytics can operate primarily on derived signals rather than raw audio.
The microphone is positioned near the agent’s mouth, and the analog signal path is designed so speech remains clean while office noise stays in the background. The gain and noise reduction parameters are set so that agent and caller voices remain intelligible without clipping when someone in the background raises their voice or a loud sound happens nearby.
The front end conditions the signal and passes it to lightweight analytics that run on the headset processor. Instead of monitoring every word, the system tracks volume balance between speakers, pitch and tone changes, silence durations, and interruption patterns. It then turns each call into three metrics, or scores, for customer frustration, agent interruptions, and extended holds.
The device sends those compact scores along with compressed call audio so supervisors can spot rising stress levels without having to monitor raw microphone feeds.
What’s Next for Always-Listening Devices
Always-listening nodes are becoming a standard for monitoring health, safety, and smart environments, but that works only if audio analytics run efficiently at the edge. Users now expect their devices to recognize spoken commands and acoustic events, so every microphone input must feed a reliable audio analytics pipeline instead of a simple audio path.
For designers, that expectation pushes more work into low-power hardware that can listen constantly in hospital rooms, industrial plants, vehicles, and buildings without overheating or draining batteries. The front end performs continuous gain control, filtering, and simple pattern detection on small processors and escalates to more complex processing only when required.[2]
These expectations make analytical capabilities a key requirement for electrical design engineers rather than a future add-on. Successful designs pair low-noise microphones with efficient and trustworthy audio front ends so that software teams can add new listening skills over the life of the device without changing the hardware.
Bringing Audio Analytics into Day-One Design Decisions
Audio analytics are no longer just an offline, after-the-fact tool; they now reside in always-listening devices. Many systems analyze sound locally to identify specific events related to safety, health, or operational quality, reducing the need to stream raw audio from the device. Regardless of the application, the same pipeline—capture, features, events—turns raw sound into decisions without streaming every waveform to the cloud.
Electrical design engineers must answer the following questions when creating a new audio design:
- Which sounds matter in an event?
- What qualifies as an event?
- Where will this node live?
- What power, thermal, and privacy limits should be considered in the environment?
- How much of the pipeline can reside in a low-power front end?
- What functions need server-class processing?
Designs that answer these questions early and pair low-noise microphones with efficient, trustworthy audio front ends give software teams room to keep adding new listening skills over the life of the device without revisiting the hardware.
Sources
[1] https://www.ideas2it.com/blogs/audio-classification-on-edge-ai
[2] https://blog.meetneura.ai/edge-audio-event-detection/
Author Bio
Traci Browne is a recognized and respected journalist and writer specializing in manufacturing and industrial applications with a focus on emerging technology, engineering, robotics, and IIoT. She has been published in Robotics Business Review, NextBot Magazine, Compoundings Magazine, Plumbing & Mechanical Engineer, Intel IQ, Professional Mariner, and Municipal Sewer and Water Magazine just to name a few. She has also written for leading cloud platform and service providers, robotics manufacturers, multi-national transport infrastructure, engineering, and constructors of civil works and buildings, as well as global technology companies.