Taking a Deep Dive into New V2X Architectures
Image Source:
metamorworks/Shutterstock.com
By Steve Taranovich for Mouser Electronics
Published March 11, 2021
Emerging vehicular networking applications, such as V2X, and use cases will need stringent Quality of Service (QoS)
requirements in latency, data rate, reliability, and communication range. Technologies often used in ultimately
developing an autonomous vehicle center around three types of sensors: camera, radar, and LiDAR. However,
vehicle-to-everything (V2X), another wireless technology that already exists, can bring significant added value to
autonomous vehicles. V2X refers to high-bandwidth, low latency, and reliable communication between a broad range of
transport and traffic-related sensors. 5G mobile networks will provide connectivity for vehicle-to-vehicle (V2V) and
vehicle-to-infrastructure (V2I) communications.
In the following, we will discuss how the 3rd Generation Partnership Project (3GPP) intends to use 5G in V2X
applications with significant advantages over current dedicated short-range communication (DSRC) or other
Cellular-V2X (C-V2X) proposals. Worth noting is that the word cellular, in C-V2X, is somewhat misleading. In this
application, cellular does not refer to a cellular network such as 5G, but instead to the technology of the basic
electronics used in cellular radios, for direct communication between two radios.
A Technology Evolution is Coming
From a communication technology perspective, future Intelligent Transportation System (ITS) services are widely
accepted. This will ultimately lead to autonomous driving and require a high level of connectivity in vehicles via
advanced communication technology such as 5G V2X. After many years of research, driven by academia and industry, and
the delivery of mature technology enablers for 5G, 3GPP is drafting the standard for 5G V2X, starting with Release
16.
Let’s first look at the definition of V2X. This vehicle-to-everything technology is a means of two-way
communication that enables the transmission of information between an automotive or electric vehicle and any
surrounding entity that might affect that vehicle. V2X applications will have an important impact on safety and
convenience well before full autonomy becomes a reality. V2X technology will also enable less gridlock, reduce
environmental impact, and add more vehicle comforts for drivers and passengers.
5G, coupled with V2X, will enhance vehicle and pedestrian safety with capabilities such as vehicle notification and
control for approaching emergency vehicles with distance/direction information, pedestrians crossing in a crosswalk
(traffic lights/signals will be controlled or extended for safety and during unexpected events, allowing the
identification and avoidance of a pedestrian darting into traffic. When an accident is near, notification of its
location and distance will be sent. Things such as school bus notifications, including unloading/loading school
children in the area, will also keep pedestrians safe.
Cellular-vehicle-to-everything (C-V2X) is a subset of V2X. It will supplement line-of-sight (LoS) sensors such as
cameras, radar, and lidar for non-LoS awareness, which is critical for safer driving. C-V2X will also enable larger
sensing coverage than LoS sensors and is the foundation for vehicles to communicate with each other along with
everything that surrounds them. 3GPP started standardization work of cellular V2X (C-V2X) in
Release 14 in 2014. It is based on LTE as the underlying technology. Specifications were
published in 2017.
The types of EV power transfer communications capabilities include vehicle-to-infrastructure (V2I),
vehicle-to-network (V2N), vehicle-to-vehicle (V2V), vehicle-to-pedestrian (V2P), and vulnerable road users like
cyclists, vehicle-to-device (V2D), and vehicle-to-grid (V2G). Figure 1.
Figure 1: The main C-V2X use cases: Vehicle-to-Vehicle (V2V),
Vehicle-to-Pedestrian (V2P), Vehicle-to-Infrastructure (V2I), and Vehicle-to-Network (V2N). V2X safety messages
may include Cooperative Awareness Messages (CAM) and Decentralized Environmental Notification Messages (DENM) in
Europe or Basic Safety Message (BSM) in the US. (Image Source: IEEE)
The automotive industry is also pursuing ways to reduce the costs for On-Board Units (OBUs) that will support 5G
V2X while avoiding/minimizing any increase of the vehicles’ prices.
5G and V2X
5G will make V2X easier, faster, and more reliable. The main difference between a 5G and V2X
framework can be summarized as follows:
- 5G, like any radio mobile service, uses an infrastructure in which the landscape is divided into individual
cells, widely overlapped, and managed by proper antenna systems, called base stations.
- V2X, like any wireless service, exhibits a more flexible structure, where small antenna-device systems, called
hot spots, assure best-effort connections by using a strong co-operation strategy.
DSRC Versus C-V2X
The high-speed communication protocols that come into play here for vehicle safety are DSRC and C-V2X. These two
protocols operate at very high speed with a high-frequency exchange of data at low latency. DSRC has a data rate of
6Mbps to 26Mbps in the 5850MHZ to 5925MHz band. C-V2x has a data rate of 26Mbps (RX) Max 26Mbps (TX). Both operate
in the 5.9GHz band, and both use the same use cases and the same message sets (SAE J2735
and J2945), and both also use digital signatures for
security and trust in message providers. DSRC and C-V2X radios do not connect, but they are broadcasting vehicle
location, acceleration, and speed while listening to other radios.
The two technologies use different wireless standards. DSRC uses WAVE IEEE
(802.11p), and C-V2X uses long-term
evolution (LTE), which cellphones use. The FCC allocated the 5.9 GHz band to
Wi-Fi and C-V2X in November 2020.
These two radio technologies cannot talk to each other, and their respective ranges are quite different. DSRC is
around 300m, where C-V2X has lower latencies, 20 percent to 30 percent more range, and performs much better in the
presence of obstructions than DSRC. Overall, C-V2X has significantly better performance. However, DSRC still does
have sufficient range and reliability for key safety applications.
C-V2X Sidelinking
5G, Release 16, brought sidelinking to industry C-V2X with 5G New Radio (NR). This release advanced C-V2X
applications such as platooning, advanced driving, extended sensors, and remote driving. Strict latency and high
reliability must be guaranteed because of the need for emergency braking and collision avoidance in critical driving
situations. C-V2X’s smallest transmission latency is at most 4ms and can be lower depending on the
implementation. It is difficult to quantize reliability here, but each new Release has added another group of
improvements in performance and safety, which has enhanced reliability. New releases are scheduled to continue on
this path of safety and reliability improvements.
The bulk of the traffic that will be carried out by short-range communications, especially in the first phase of
V2X deployment, will be periodic broadcasting messages by each vehicle communicating its status and movements.
In dense traffic areas, available channel resources will saturate and lead to an increase in packet losses. This
could endanger driver and passenger safety. Congestion-control algorithms were examined and defined to modify
certain parameters before these conditions reach critical levels. However, instead of looking at specific
algorithms, researchers examined the Wi-Fi standard approach (IEEE 802.11p) versus the cellular standard approach
(sidelinking LTE-V2X as defined by 3GPP as part of C-V2X in Release 14).
The C-V2X communication technology was developed by 3GPP to enable direct communications among vehicular user
equipment (VUE) over the sidelink, also named PC5 interface. C-V2X sidelink is the first wireless system to
introduce distance as a dimension at the physical layer. This will enable achieving a uniform communication range
across widely varying radio environments for both LoS and non-LoS.
C-V2X includes two modes of communication from Release 14:
direct mode (PC5) for the most immediate and
latency-sensitive communications, and network mode (known as Uu)
since it links User Equipment to the UMTS Terrestrial Radio Access Network. It uses an existing cellular network for
broadcast-type communications.
For the PC5 mode:
- Mode 3 (scheduled) in which the sidelink resource assignment is performed with the supervision of the eNodeB
and requires cellular infrastructure support for radio resource management.
- Mode 4 (autonomous), where resource and interference management is performed by vehicles in a distributed
manner and does not involve cellular infrastructure (and can be used in areas without cellular coverage).
Security and Privacy in V2X Communication
LTE-based V2X communication uses a high capacity, large cell coverage range, and widely deployed infrastructure to
support various types of vehicular communication services for safety and non-safety applications. Technical
organizations such as 3GPP and Qualcomm have already prepared the roadmap toward 5G-based V2X services.
Security defined in 3GPP mainly includes confidentiality, integrity, authenticity, and resistance to replay attack.
New privacy and security challenges, including secure mobility management for group-oriented autonomous platoons,
reliable cooperative driving, efficient and privacy-preserving vehicular big data sharing and processing, and more,
demand more investigation in 5G vehicular networks.
In the scenario of the possible solutions for automotive security and safety assurance against any cyberattack, the
full adoption of a double-key
cryptosystem is advisable.
V2X applications depend on continuous, detailed location information, which can lead to privacy concerns. In a
privately owned vehicle, location traces will reveal the movements and activities of the driver, who might or might
not be the owner of the vehicle. In short, sending and disseminating V2X user location information might have a
possible privacy concern for the owner and driver of the vehicle.
Other V2X applications include communication between vehicles that will augment existing methods to help with left-
or right-turn assistance, emergency braking warnings, and improved situational awareness at intersections. Extending
Waze concepts can control or suggest
speed adjustments to account for traffic
congestion and update a GPS map with real-time updates on lane closure and highway construction activity. V2X in
some form is essential to support over-the-air (OTA) software updates for the now-extensive range of software-driven
systems in your car, from map updates to bug fixes to security updates and more.
V2X safety messages can be made to include a Basic Safety Message (BSM) in U.S. standards or Cooperative Awareness
Messages (CAM) and a Decentralized Environmental Notification Messages (DENM) in a European Union (EU) standard.
BSM contains position, velocity, and acceleration information and is transmitted up to 10 times per second. This
message system also enables the vehicle receiving unit to predict collisions and warn the driver.
V2X Message Protection and Security
V2X and V2I communication need strong security to protect messages against fraudulent or misleading use that might
lead to safety and privacy issues. Another method for security is signed messages using Public Key Certificates that
are used to prevent unauthorized parties from interfering with the exchange of data and to pseudonymize the
communication securely.
Public key infrastructure (PKI) consists of policies and procedures used to create, manage, use, save and revoke
digital security certificates. PKI allows for the transfer of electronic information securely and
goes beyond just passwords as authentication with a requirement of more rigorous identity confirmation.
5G New Radio (NR) Intention Sharing
Intention or trajectory sharing will enhance autonomous driving by providing a higher level of predictability and
traffic efficiency in advanced path planning.
5G New Radio (5G NR) will enable intent sharing with:
- High throughput: 5G can provide the required high data rates needed, such as greater than 100Mbps in a 1km
stretch.
- High reliability: 5G can ensure that trajectory information will be shared accurately and promptly.
- Low latency: 5G low latency capabilities will allow trajectory information to be shared within a few
milliseconds.
C-V2X Performance in Crowded Highway Situations
The 5G Automotive Association (5GAA) ran V2X performance and functional tests in a test report entitled V2X
Functional and Performance Test Report, in which C-V2X technology was tested for a highly congested scenario
in a laboratory setting. Even in this congested scenario, C-V2X latency remained bounded by the 100ms latency budget
configured for that scenario, which is a very positive result.
In a series of laboratory and field tests, it is observed that:
- C-V2X communication in 20MHz CH183 has the same reliability performance (Packet Reception Ratio vs. distance) as
the identical BSM-like message transmission in 10MHz CH184.
- Impact of C-V2X high load transmissions in CH183 on DSRC basic safety transmissions in CH172 is negligible up to
a 1.4-km range in Line of Sight (LOS) conditions.
- Impact of C-V2X high load transmissions in CH183 on V2I and I2V transmissions in CH178 is negligible up to a
1.4-km range in LOS conditions.
- Impact of C-V2X high load transmissions in CH183 on V2I and I2V transmissions in CH180 is negligible up to 1km
in LOS conditions.
Ford and Qualcomm performed additional field tests supporting the latest 5GAA petition for waiver with the Federal
Communications Commission (FCC) for C-V2X deployment. Those tests by Ford showed C-V2X with a very acceptable
performance, especially in LOS conditions.
According to the 5GAA website, C-V2X was deemed ready for deployment with commercial chipsets and was also seen as
ready to start in-vehicle deployment in the 2020/2021 timeframe globally. The 5GAA will partner with the relevant
Standards Developing Organizations (SDOs) to drive the requirements of 5G V2X to create a successful V2X ecosystem.
Conclusion
The FCC effectively changed the vehicle communications Cooperative
Intelligent Transport Systems (C-ITS) market in the U.S. via the restructuring of the 5.9GHz band.
The automotive industry must go forward on a narrowed spectrum with C-V2X technology instead of the widely used
Dedicated Short Range Communication (DSRC). The changes announced pave the way for progress, eliminating the
uncertainty caused by competing technologies.
V2X and 5G are fast-becoming integral technologies for automakers as it endeavors to commercialize
fully autonomous vehicle technology in the years ahead. After the launch of C-V2X vehicles in China in
2021, Ford anticipates bringing the technology to all of its vehicles sold in the U.S. beginning in 2022. The 5GAA
will partner with the relevant SDOs to drive the requirements of 5G V2X to create a successful V2X ecosystem.
IHS Markit, a financial services company, posted an analysis on 5G, C-V2X, and
automotive connectivity for the 2021 year on its website in January 2021.
According to a news release about a C-V2X study published on Market
Watch:
“The V2I communication segment is expected to grow at a CAGR of over 12% over the forecast period due to the
increase in the adoption of smart traffic infrastructure. The smart traffic infrastructure involves smart traffic
signals and smart surveillance cameras, which communicate with vehicles to provide information about traffic and
road conditions.”
More exciting vehicle advances are coming, which will significantly change the way we drive our vehicles for the
better.
Author Bio
Steve Taranovich is the author of the
non-fiction “Guardians of the Right stuff”, a true story of the Apollo program as told by NASA and
Grumman Corp. engineers, an astronaut, and technicians. Steve was the Experienced Editor-In-Chief of EETimes/Planet
Analog and Senior Technical Editor at EDN running the Analog and Power Management Design Centers from 2012 to 2019.
He has a demonstrated history in electronic circuit design and applications for 40 years, and 9 years of technical
writing and editing in industry. His specialties include Analog Electronics, Space-related Electronics, Audio, RF
& Communications, Power Management, Electrical Engineering, and Integrated Circuits (IC). Steve
Taranovich is a strong media and communications professional with a BEEE from NYU Engineering, 1972, and an MSEE
from Polytech University in 1989. From 1972 to 1988, he worked as a circuit design engineer in audio (8 years) and
microwave (8 years).